Issue
The customer can log off of Continuum, but he can't shut down Continuum.
Environment
CyberStation
WebClient
Cause
Permission to exit Continuum has not been granted to the Continuum User.
Resolution
- Right click on the Continuum icon in the Windows Active Icon tray
- Select Security
- Navigate to the appropriate object class or folder. In this case navigate to the Miscellaneous folder.
- Look for the row named Terminate Continuum.
- Move left horizontally along the row until you get to the icon associated with the user group you wish to grant the permission to. (The user group indicator will appears when the arrow is over each lock or key icon).
- If there is a lock icon, the permission is currently denied. Click on the lock and the icon changes to a key. The permission is now granted.
- Log Off of Continuum and log on with a user from the modified user group to test the permissions.
NOTE: There are cases when multiple permissions must be granted to allow a user to access specific functions. For example, you can grant a user permission to reload a controller, but he will not be able to do so unless you have granted him access to launch Continuum Explorer.