Issue
Having trouble Linking to a File from a TMGL Graphics page in Vista Workstation
Environment
TGML
Vista Workstation
Cause
Most likely cause is not using the correct button type or script feature. Below is the most basic means to link to a file.
Resolution
- Add the "FileButton" object found in the Basic Controls Component Library to the TMGL file
- Select the object
- In the Properties Window, scroll down to the heading "Custom" and the property "File"
- Type in the complete path and filename. Example C:\Vista_Files\TGML.pdf
- Save the TGML graphics page
- Test the link in Vista workstation