Issue
User limitations in a Xenta Server
Environment
Xenta Server
Cause
Setting up User rights on a Xenta Server
Resolution
Web Users:
- Web Users are created only from the Web Interface, not XBuilder
- The limitation on web users is based only on available controller memory
- A normal user should use less than 100 bytes
- Excess numbers of users will limit your potential use of controller memory
Simultaneous Users:
- In XBuilder, click on the Xenta Server object
- Scroll down to TCP/IP Settings and select "Max. number of HTTP sessions"
- the default if 15, but this number can be modified to between 10 and 20 users.
FTP Users:
- In XBuilder, click on the Xenta Server object
- Scroll down to FTP settings and select "Max Users"
- The default number is 4, and the maximum is 5 users.