Issue
How do I upgrade a CX9400 to a 9680?
Environment
- Continuum
- CX9400
- 9680
- Windows XP
- Windows Server 2003
- Windows Server 2008
Cause
Continuum Versions 1.90 and below do not have a direct procedure for upgrading a CX 9400.
Resolution
Upgrade Continuum to 1.91 or above which allows a selection to upgrade the CX 9400 to 9680. This procedure makes the appropriate changes to the database.
Upgrading a CX 9400 without the direct convert option (Continuum 1.90 or less) has to be done manually by exporting and importing dump files. There are a differences between these 2 controllers and there is a potential for database problems. Manual manipulation requires a large amount of work which takes a considerable amount of time.