Issue
A new Lookup table has been created, when should it be downloaded?
Environment
Sigma 4.03
X32 and X96 controllers
Cause
What is the correct sequence for downloading new Lookup tables?
Resolution
The download process is as follows;
1 - Create the new lookup table with the required configuration, using the Sigma System Setup.
2 - Allocate the new lookup table number to the appropriate Sigma object and then download it.
3 - In the Sigma System Diagnostics, select the correct controller number, and then choose to "Build and Download Lookup Table". This process will create a new "Lookup.rec" file in the OSN??? folder, and this will contain the new table and any others required by the controller.