Issue
If airflow direction is reversed in duct from f.ex. 100 Pa to -100 Pa, will the SPD310/SPD360 break?
Environment
- SPD310
- SPD360
Cause
Reversing airflow direction in duct.
Resolution
It will not break.
If the "sym" jumper setting is changed when airflow direction is changed (reversed), it will read the value correctly.