What is the LCD password on the Infinity SCX920 and LCX810 Controllers?

Issue

How to find out or set the LCD password on old Infinet controllers with LCD displays

Product Line

Andover Continuum

Environment

Infinet LCX810 and SCX920 controllers with LCD Displays

Cause

Current documentation on the Extranet does not define what the password is or how to set it.

Resolution

The system variable "LCDPassword" determines what the password will be, this can be changed as required.

The default is 123 then press Enter.