CyberStation SQL collation

Issue

What SQL collation is supported by CyberStation

Product Line

Andover Continuum

Environment

CyberStation

SQL Server

Cause

To know if any other SQL collations are supported by CyberStation.

Resolution

Only the SQL_1xCompat_CP850_CI_AS collation has been tested with CyberStation.

Note that in more recent versions of SQL server (i.e 2005) you can have the Collation on a per database basis so ContinuumDB will have its collation set to SQL_1xCompat_CP850_CI_AS and another database can use a different collation setting.