Issue
Upgrading / downgrading a jar file in I/A Series G3
Environment
Niagara G3 (all version)
Cause
Not applicable
Resolution
Do the following:
1. Shut down Workbench
2. In Windows Explorer, navigate to the C:\Niagara\<release>\modules directory
3. Find the original module (e.g. tacAsd.jar), and rename it (e.g. tacAsd.old)
4. Copy the new module in to the modules directory
5. Re-open Workbench, then go to Platform > Software Manager
6. Highlight the module (e.g. tacAsd.jar), then click Install, then click Commit
7. The module will be installed, and the ENC will re-boot