Project Builder File Will Not Open

Issue

Executing a Project Builder File should launch Visio and open a drawing. Instead, Visio opens but stops short of the file opening.

Product Line

TAC Vista

Environment

  • Project Builder
  • Visio

Cause

Project Builder is disabled in Visio.

Resolution

  1. In Visio go to Help>About Microsoft Visio
  2. Click on Disabled Items button in the pop up.
  3. Ensure Project Builder is not listed
  4. If so, select the Project Builder Listing
  5. Click the Enable button.
  6. Restart Visio.