Issue
How many additional workstations can connect to a Continuum standalone system?
Environment
- SA CyberStation
- MSDE
Cause
Using Continuum stand alone installation as a database server for additional workstations.
Resolution
Stand Alone key is for 1 Cyber.
MSDE supports up to 3 users, but a LAN key is needed with more than 1 Cyberstation.
To upgrade SA to LAN, the Stand Alone key must be upgraded with a cookie.
The Stand Alone machine with the database should have the SA key, up to two additional machines can use the Stand Alone machine as their database server. The additional machines need LAN keys.