Issue
- Graphics points appear OK, but are not dynamically updating. Alarms and messages appear in the AMT.
- Double clicking on a point on the graphics, the displayed value is significantly different to what is displayed on the graphics page.
- Graphics have question marks for the data. Rebooting the PC makes data viewable again on the graphics. This happens regularly over time.
Product Line
TAC INET
Environment
I/NET Seven 2.15B through to 2.30
Cause
Changes in Microsoft Windows video/graphic files have meant changes were required to the I/NET Seven Software.
Resolution
Upgrade your I/NET Seven system to 2.31 or above.