B_Link Fiber devices cannot be used on the IP network

Issue

Can B_Link Fiber devices be used on the IP network?

Product Line

Andover Continuum

Environment

  • Network Topology
  • Windows XP
  • B-link Repeater
  • BCX 4040
  • B4920
  • BACnet Repeater RS-485

Cause

Configuration of Fiber Network

Resolution

No. The B-Link Repeater is used on the RS-485 Network not IP.