Cannot delete personnel profiles

Issue

Tried and cannot delete personnel profiles from personnel manager.

Product Line

Andover Continuum

Environment

Continuum 1.81

Cause

Personnel profiles have become corrupted and can't be deleted
You can not rename areas without removing/ replacing them in the profile.

Resolution

Procedure to remove corrupted personnel profiles:
1. Start Continuum
2. Run ACDEVApp.exe from the Continuum directory.
3. Click Generate.
4. replace the 3 lines:
 .      <REQUESTOPERATIONS>
 .      </REQUESTOPERATIONS>
 .      </IACDEVREQUEST>  
            with the following 6 lines, only replace the word ProfileName with the name of the profile being deleted      
 .      <REQUESTOPERATIONS>
 .      <DELETE>
 .      <OBJECT PATH="ProfileName"/>
 .      </DELETE>
 .      </REQUESTOPERATIONS>
 .      </IACDEVREQUEST>

 

5. Press the "Process Request" button