How to add additional fields to the New Search window in the Personnel Manager?

Issue

The New Search window shows a set of predefined attributes to search on, can additional attributes be added to this list?

Product Line

Andover Continuum

Environment

Cyberstation Personnel manager, Versions 1.80 and above.

Cause

There is no option to add/ remove fields from the New Search window.

Resolution

1) The New Search Window entries are fixed, there is no option to add / remove fields in this window.

2) To search on one of the other attributes not listed; use a List View of Personnel to show the required attributes and use a Qualifier on that attribute to prompt the user for the search criteria.

3) The * character can be used as a wildcard, so for example if searching on the Vehicle Info attribute entering Ford* would find all Ford vehicles if the field is used to hold the make & model of vehicles.