Issue
Cannot open Create/Edit Badge in Personnel Manager even though badging is enabled on Security Key
Getting error message "Cannot init license"
Environment
Continuum Personnel Manager
Cause
Windows user does not have enough permissions to run EPI Designer (EPI the Print/Badge Program installed with Continuum)
Resolution
Change the Windows login to one that has sufficient permissions to run EPI Designer (the Print/Badge Program)
The standard Windows User does not have permission to run EPI Designer (the Print/Badge Program) whereas a standard PowerUser or Administrator does have permission.
NOTE
This was an Windows XP issue, similar issues may still be present in newer Windows versions
Continuum v1.92 was used for this document