Issue
Can I change the display of an attribute using the old Personnel Editor or in the Personnel template editor
Environment
Continuum Cyberstation
Cause
Change the display of a personnel attribute.
Resolution
The old personnel editor or the personnel template editor there is no way to change the attribute name. In the new Personnel Manager you can change the display of an attribute name.
Example: Changing attribute Info1 to BuildingNumber
- Open up a personnel record
- Select configure and select customize attributes
- Select the display name for the attribute to be changed
- Change the display name and select Ok.