Issue
TAC Vista Web Settings > Preferences > Login and Logout > Automatic Logout
(An inactive user is automatically logged out after a specified period of time)
Selection for automatic logout time is restricted to 5, 10, 15, 20, or 30 minutes.
- Set the logout time to less than 5 minutes
- Set the logout time to more than 30 minutes.
- Customize the logout time to something other than specified intervals.
Environment
- Vista 5.1.5
- Webstation
- TAC Vista Web Settings
Cause
Selection for automatic logout time is restricted to 5, 10, 15, 20, or 30 minutes.
Resolution
- Navigate to C:\Inetpub\wwwroot\TACVistaWeb515
- Open the file web.config. Use, for example, Notepad2 (Do not use wordpad as it formats the file differently)
- Search for "sessionState"
- Change the "Timeout" for the SessionState to the desired logout time in minutes
- Save the file