Issue
The error "Security error: security logon rejected" is received when accessing schedules in webclient
Environment
- webClient
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
An "&" (ampersand) that is used in a logon name or password or another object will cause problems with webClient
Resolution
Do not use the ampersand, change the object name or username to use a different character.