Continuum Software Download

Issue

Can the Continuum Software be downloaded from the web, or ordered on CD?

Product Line

Andover Continuum

Environment

Continuum Cyberstation software

Cause

Download of Continuum Cyberstation software

Resolution

The Continuum Cyberstation software is available for download from The Exchange Download Center. The link below will direct you to the Cyberstation software.

CyberStation Software

If specific older versions of software are required see Lessons Learned #5721.

If a customer specifically requests the software on a CD, then these can be ordered through the regular Order Entry channel specifying the version required.