Issue
-
How to monitor if an HOA switch in an I/O module for a Xenta Server is set to something other than auto.
- How to tell if an I/O signal is hardware (HW) overridden/forced
Environment
Xenta Server (731, 721, 711, 701)
Cause
Some I/O modules have switches that can be used to manually force/override the outputs.
It could be important to know what signals are forced.
Resolution
In XBuilder, each physical I/O that has a manual switch also has a signal for it.
This can be used to monitor the switch.