Issue
The I/A Series R2 (Niagara) build 529 programLib jar file is missing 5 objects that were available in
previous build programLib-2.301.527c.v1.jar.
The missing objects include:
- ConfigurableBinaryOutputNode.class
- FlexLimitEnableBits.class
- FlexString.class
- Bpa2Str.class
- Fs2Fp.class
Environment
I/A Series R2 (Niagara) build programLib-2.301.529.v1.jar
Cause
Objects listed were not included in programLib-2.301.529.v1.jar
Resolution
The missing objects were restored in the programLib-2.301.532d.jar. Use it instead of the programLib-2.301.529.v1.jar.
- In Windows Explorer, rename programLib-2.301.529.v1.jar. to programLib-2.301.529.v1.jar.old in the emb, nre/modules, and nt directories.
- Download programLib-2.301.532d.jar
- Copy into all three 2.301.529.v1 directories (emb, nre/modules, and nt ).