Issue
Under certain unknown scenario reloading a b3 device may result in CyberStation hanging when setting the attributes of the first object to be reloaded.
A buffer overrun error may also appear.
Environment
- CyberStation
- bCX4040
- b3
Cause
Invalid BACnet device configuration in database.
Resolution
- In CyberStation go to the BACnet Devices folder and delete the BACnet device for the b3.
- Perform a Find New BACnet Devices.
- Send the BACnet device for the b3 to the database
- The reload operation should now complete successfully.