Issue
When the Update TAC network is selected from the System Plug-in LNS objects are not updated in the TAC Network View
Only Xenta devices are updated.
Product Line
TAC Vista
Environment
TAC Vista 5.xx System Plug-In
Cause
The "Include LonWorks devices" is not checked in the TAC System Plug-in.
Resolution
To correct the LNS objects failing to be updated in the TAC Network, carry out the following steps:
- In the TAC System Plug-in select the TAC Network from the tool Bar.
- Select the setting option
- Ensure the "Include Lonworks devices" option is checked as shown below.