Issue sizing photo in Personnel Manager or photo not filling the photo frame completely.

Issue

Blank space in personnel photo, photo does not fill the photo area.

Product Line

Andover Continuum

Environment

CyberStation

Cause

No cropping in photo capture adjustment.

Resolution

1. In the adjust section in the Capture Photo dialog, set the appropriate cropping and/or photo size.

2. In the Image Enhancement dialog, select the area in the original image (typically a rectangle around the person's face) that will appear in the photo frame.