RS-232 converters to RS-485

Issue

Can I use a RS-232 converter to RS-485

Product Line

Andover Continuum

Environment

Modbus

Cause

Using a converter for RS-232 to RS-485

Resolution

RS-232 converters to RS-485 have been reported to work in some cases, we do not support converting RS-232 to RS-485.

There are a lot of different configurations that can be different from vendor to vendor that can cause communications issues. It is suggested to use a commport that can handle the particular protocol that is needed instead of using a converter to change the protocol.

Another option is to use our own Infilink200 or B-Link as an RS-232 to RS-485 converter for use on Comm1 when loaded with an Modbus RTU Xdriver or similar RS-485 protocol.