Modbus Float type polling using special function codes

Issue

How to read float type point using an Xdriver

Product Line

Andover Continuum

Environment

Modbus

Cause

Which Xdriver function code to use.

Resolution

When polling for a point of Float type and using the Xdriver. Use one of the Special function codes available in the Xdriver parameter list. For Float type use function code 245 or 248.