Launch Vista System Plug-In in LonMaker/Visio 2010

Issue

How to launch the Vista System Plug-In in Visio 2010.  In earlier versions, it was located under the toolbar menu LonMaker > System Plug-Ins, but that menu item no longer exists.

Product Line

TAC Vista

Environment

  • LonMaker Turbo 3.2
  • Visio 2010 Add-Ins

Cause

Usual drop-down tool bar menu items do not exist in Visio 2010 as they did in earlier versions.

Resolution

System Plug-Ins can be found under the Add-Ins tab

  1. Add-Ins
  2. LonMaker
  3. Network Plugins.

If the Add-Ins are missing, please see Lessons Learned Article #2811.