Is ok to change IP port for TAC Vista Webstation?

Issue

Customer need to change TAC Webstation to use another port then the default port 80

Product Line

TAC Vista

Environment

TAC Vista 5.1.5

Cause

TAC Vista Webstation is using the port defined by the IIS

Resolution

Change port in the IIS.
 

  1. Open properties for the Default website
  2. Change the TCP port