Issue
What hardware is necessary to integrate an I/NET security system with a Vista front end?
Environment
Vista 4.5.0
Vista 5.x.x
Xenta Server 527
Cause
To properly integrate an I/NET security system to Vista a Xbuilder project must be used to expose the I/NET controllers in the Vista tree structure. In addition the unit must not block AMT (Alarms, Messages, and Transactions) traffic from the I/NET controller LAN.
Due to these requirements the Xenta Server 913 and the Xenta Server 527-NPR do not meet the requirements to integrate an I/NET security system into Vista.
Resolution
Use a TAC Xenta 527 (part number 007308200) for integration of an I/NET security system to Vista.