Issue
How to modify or add an area or areas to selected personnel
How to modify personnel (or other) attributes
Environment
Cyberstation Personnel Listview Attributes Editlock lock locked
Cause
Need to add or delete areas from multiple personnel
Need to change attributes
Resolution
- Create a listview of personnel, with a filter (for example, by department) to show only the personnel to be modified.
- Select the personnel to be modified.
- Right click on the selected Personnel objects and select "Add Areas" or "Remove Area" from the context menu.
- In the ‘Area’ window you can select one or more areas to assign.
- Other attributes can be modified in the same manner EG. if many objects get edit locked, select all in the listview, then right click, set attribute, Edit lock to false.