Replacing a Satchwell MBF 2730 2 1/2 3-Port valve.

Issue

Replacing a Satchwell MBF 2730 2 1/2" 3-Port valve with a current version.

Product Line

Field Devices

Environment

MBF 2730

MBF 4732.

Cause

The Satchwell MBF 2730 was an imperial valve and the replacement MBF 4732 is metric, so there will be differences in size.

Resolution

The Satchwell MBF 2730 was an imperial 2 1/2" valve, this valve is replaced by a MBF 4732 65mm version, therefore there are some differences in size, the following table shows details of this valve.

 

 Below are details of the current range of MBF valves.