Firmware version and bootloader version do not match

Issue

Why do the Firmware version and bootloader version do not match

Product Line

Andover Continuum

Environment

BCX

B3

Cause

Verification on why the two do not always match.

Resolution

When firmware versions (application firmware files) are posted to the web, they do not always included the associated bootloader version. The reason for this is that rarely is a bootloader version changed. When bootloader versions do change it will be announced in the release notes for the particular firmware version.