Issue
Sigma Web Graphics must be installed as an Administrator, but most users do not have these rights.
Environment
Sigma
Sigma Web Server
Cause
As most network users do not have Admin rights, there is a need to install Sigma Web Graphics across the network.
Resolution
The following text has been provided by the Sigma programmers and should be understood by the IT professionals.
First you need to create a response (answer) file
Then play back the response (answer) file in silent mode
To review the InstallShield Setup Parameters.pdf, please Click Here.