Issue
At times running a vbscript from webpinpoint is needed and you may receive an error after configuring the button that webpinpoint cannot find the vbscript you are trying to run.
Environment
Webclient
Windows XP
Windows Vista
Windows 7
Windows Server 2003
Windows Server 2008
Cause
There is some configuration and file placement required to get this to work.
Resolution
Create a button on a graphic in Continuum and set it up as follows: Action Start windows program Windows Program c:\windows\system32\wscript.exe Command line argument (Hello.vbs is an example script) Hello.vbs (This is the vbscript you are trying to run) If you only place hello.vbs in the system32 folder you will get an error when pressing the button in webpinpoint that it can’t find c:\program Files\Webclientpinpoint Copy hello.vbs to c:\program Files\Webclientpinpoint The script should now launch. Caveat: This was a very basic test, not all vbscripts may launch depending on their content.
Warning! Allowing vbscripts to run in IIS and on websites is potentially dangerous because viruses and malicious software can be introduced this way.