Issue
When an alarm arrives at the Alarm Manager, it is highlighted and can be acknowledged. If the mouse is clicked elsewhere the focus is lost from the alarm. Selecting the Alarm Acknowledge button now does not re-select the alarm as it did with the BAS2800+ system.
Environment
Sigma all versions.
Cause
Alarm acknowledgement and focus was changed between BAS2800+.and Sigma by design.
Resolution
The Sigma alarm acknowledgement is as designed. Un-acknowledged alarms can be highlighted again by selecting update alarm totals.