Issue
When configuring an Infinity Schedule, why can't I select an object from another controller for the Occupancy Point?
Environment
- Continuum
- CyberStation
- WebClient
- Schedules
- InfinityController
Cause
Trying to configure a schedule to control a remote point.
Resolution
- Infinity Schedule objects must control points that reside in the controller in which the schedule resides.
- Continuum will not allow you to browse to or select points that reside in controllers other than the controller that the schedule resides in.