Issue
Decoding information from the door's DoorFault attribute value.
Product Line
Andover Continuum
Environment
- CyberStation
- CX9702
- CX9680
- ACX5740
- ACX5720
- ACX701
- ACX781
Cause
The door's DoorFault attribute value is a weighted bit map that encodes information about a problem with the door as a whole or with one or both sides of a single reader/dual reader door.
Resolution
The attribute is a bitmap that contains the following data:
BIT | VALUE | DESCRIPTION |
1 | 1 | ACX Database Fault |
2 | 2 | Entry Keypad Tamper |
3 | 4 | Exit Keypad Tamper |
4 | 8 | Entry Reader Bit Fault |
5 | 16 | Exit Reader Bit Fault |
6 | 32 | Bond Sensor Violation |
7 | 64 | Unused |
8 | 128 | Unused |
For example, a value of 2 indicates a keypad tamper at the entry reader, a value of 4 is a keypad tamper at the exit reader, 6 is keypad tamper at both readers and so on.
Note: The AlarmEnrollment Alarmed Attribute has a dropdown box that includes Doorfault. Ignore that. Set The AlarmEnrollment Alarmed Attribute to be Value and the Expression to be DoorFault = 2 in order to alarm a keypad tamper at the entry reader.