Issue
Is a license required for the S4 BACnet to N2 Routers?
Product Line
TAC I/A Series, Field Devices
Environment
- S4 BACnet to N2 Router-16
- S4 BACnet to N2 Router-32
- S4 BACnet to N2 Router-64
- S4 BACnet to N2 Router-128
- S4 BACnet to N2 Router-256
- I/A Niagara R2
- I/A Niagara G3
- I/A BACnet
- Metasys N2 network
Cause
Additional information on 3rd party router
Resolution
No license is required. But you will need to fill out the S4_Group_Order_Form and send it to CCC at the time of ordering.
Link to S4 BACnet to N2 Routers for additional information