Issue
When opening Lonmaker a license error indicates that the license has not been activated or expired.
LonMaker License Wizard
This license has not been activated, or has expired. Applications using the license will not function unless you register the license.
The information below shows the current usages for this license. Click Next> to activate the license:
Product Line
TAC Vista, Other
Environment
NL220
Lonmaker
Cause
Corrupted LNS Credits on your PC
Resolution
Occasionally, software errors may prevent the licensing mechanism used by the LonMaker tool or LNS Applications from working properly.
Use the license checking procedure below to locate your license problem, then download and install the LNS License update 2006
This will NOT fix your already corrupted license files; however, this will help prevent the license from becoming corrupted in the future.
To fix the problem, use one of the following procedure :
Procedure -- Checklic command:
- Open a Windows command prompt. To open a command prompt, click Windows Start > Run, and type cmd for Windows XP and Windows 2000, or type command for Windows 98. Then click OK.
- Type in the following commands, depending on the software product you are fixing (you can execute this command from any location). Press the Enter key at the end of the command:
Product |
Command |
LNS Application |
checklic nsseng.exe |
- An example of a working license is shown below.
C:\>checklic nsseng.exe
If you get an error in this screen Click Here for a list of errors and related repairs.