Issue
DCom or other error message seen when running CyberStation
Extended logging errors may be seen
Error connecting to database may be seen, but CyberStation still runs up
Alarms not getting to Active Alarm window
Environment
Continuum
Cause
An unspecified PC error, or Continuum Workstation error has occurred such that the CyberStation does not connect to the database correctly.
This may be a sign of a more serious fault with the PC (hard disk, RAM fault, CyberStation installation error) but this would require further investigation.
Resolution
1. If possible re initialize the database (all CyberStations need to be shut down before this is started. For a LAN install use "Server" or for a single User install use "Stand Alone")
2. Re initialize the workstation (first close the CyberStation), then test by running the CyberStation