Can an existing UNC-600 serve graphics for a new UNC-520, without adding an Enterprise Server?

Issue

Can an existing UNC-600 serve graphics for a new UNC-520, without adding an Enterprise Server?

Product Line

TAC I/A Series

Environment

I/A Series (Niagara) UNC-600

I/A Series (Niagara) UNC-520

Cause

Application for serving graphics without adding Enterprise Server.

Resolution

Yes you can without adding a Enterprise Server.

It is recommended that native Niagara objects in the UNC-600 be liked to data points in the UNC-520. This will optimize communication speed and database modifications if need.

Remember to set-up the address book and select PEER to PEER. And to watch the resource count of the UNC-600