Issue
Programs don't work in an i2 controller after being copied from another working controller.
Environment
- CyberStation
- Plain English
- Plain English
- InfinityPrograms
Cause
Programs not working properly in an i2 Controller.
Resolution
When dragging objects from one controller to another...
- Do not drag the source InfinityController onto the target controller. Rather, from the object view window, select all objects in the source controller and drag them to the target controller object.
- From the Options menu in Continuum Explorer, under the Name Conflicts tab, make sure the first four options are checked.