Issue
I cannot connect to a b3 controller, even when it is removed from the MSTP bus.
I cannot connect to an Infinet controller, even when it is removed from the Infinet bus.
Environment
- Continuum
- Roam IO
- MSTP
- Infinet
- i2
- b3
Cause
Need to connect with a local controller using RoamIO.
Resolution
- In some cases we have found that RoamIO has trouble connecting to an individual i2 or b3 controller.
- If you are having trouble connecting via RoamIO to a controller that is not connected to the controller bus, try connecting two controllers together and attempting to connect.