Issue
The default font size in the TGML Graphics Editor is 15. Can this value be changed?
Environment
TAC Vista - TGML Graphics Editor
Cause
Default Font Size in TGML Editor is 15 and it is hard coded in the software.
Resolution
It is not possible to modify the default font size. When we change the font size, the TGML editor automatically remembers the last value used.