Issue
Plug-in will not launch. Results in error "Active X: could not create object"
Environment
- Windows 7 32 bit
- Windows Vista
- NL220
- LonMaker
- Vista Plug-ins
Cause
Needs to be run as an administrator.
Resolution
- Verify Administrator account is logged in.
- Install Toolpack (or hotfix) as administrator
-
Take note of the installation location, and go to this folder after the installation of the hotfix.
The default location for these plug-in application files is:
C:\LonWorks\apps\TAC - Run file: TACXenta102AXPlugIn.exe, as administrator and click Deregister Plug-in, then Register Plug-in.
- Open NL220 or LonMaker and register the Xenta 102-AX plug-in.