Issue
WorkPlace Commissioning Tool is displaying third party devices in red.
Product Line
TAC IA Series
Environment
I/A Series WorkPlace Commissioning Tool
Cause
When the WorkPlace Commissioning Tool discovers a device (if Extended Data in selected) it will display the devices name as learned from the device. If a device name is not unique it will be displayed in red.
Resolution
Displaying the devices in red does not suggest trouble, but rather indicates duplicate device names were discovered
(see F-27358 WorkPlace Commissioning Tool and Flow Balance Tool Users Guide Chapter, "Device Icons").
The device name assigned by a third party manufacturer is not something the WorkPlace Commissioning Tool is designed to alter.