Issue
Each Cyberstation has a path to pinpoint graphics and the graphic file could be different on each Cyberstation. A way is needed to access and update one set of pinfiles.
Environment
- Continuum
- Webclient
- Windows XP
- Windows Vista
- Windows 7
- Windows Server 2003
- Windows Server 2008
Cause
Configuration is needed to allow updating and accessing one set of pinpoint files.
Resolution
- Share a folder (Microsoft sharing and permissions) on one Cyberstation or Server that will contain the Pinpoint graphic files (including backgrounds and images)
- Copy all edited pinpoint and graphic files needed to the shared folder
- Go into Pinpoint on each Cyberstation and go to the View > Options
- Edit the Graphic, Image and Background paths to point to the shared folder.
- Once there are not Red Xs, the path has resolved and pinpoint will then use that folder for its graphic files on that Cyberstation