Issue
Doing a Niagara G3 integration with a Modbus controller from ASCO Power Technologies. What type of Niagara object is required to read register 40158?
Click here to view Modbus Register Map
Environment
Niagara G3
ENC-520
ASCO Power Technologies controller
Cause
Cannot identify what type of object is needed.
Resolution
The number appears to be an enumerated value (1-22) and is a read-only integer.
Use a Numeric Point.