Filter output window in XBuilder to view Errors more easily

Issue

The output window in XBuilder will show three different message types:

  • Info
  • Warning
  • Error

If an error is occurring during a Generate command, it may be difficult to locate the exact error in and among hundreds of warnings.

Product Line

TAC Vista

Environment

XBuilder

Cause

The "Previous Error" command when right-clicking in the output window will take into account both Warnings and Errors.

Resolution

  1. Right-click in the output window of XBuilder
  2. Expand the Filter Messages option
  3. Uncheck the options for
    "Show Info Messages" and
    "Show Error Messages"
  4. The output window will now only show true error messages and it will be much easier to determine the error that is stopping the generate command from completing.